Join us at Elevate Live! in Las Vegas or online June 12-16.  Register Now

Guide

Are You Getting the Most Out of Your e-STUDIO Device?

Toshiba / April 20, 2026
A Toshiba employee reviewing a manual.

If your office relies on a Toshiba e-STUDIO MFP, you already have a powerful tool at your fingertips. But for most teams with one to five devices, usage rarely goes beyond the basics. Print. Scan. Maybe copy.

That leaves a lot of value on the table.

Many of the most useful e-STUDIO features are built in and ready to go, yet they often go unnoticed. These features are designed to simplify everyday tasks, reduce manual work, and help your team move faster without adding complexity.

Here are a few worth putting into your daily workflow.

Simplify large and scanning jobs

Not every document is neat, stacked, and ready for the feeder. Contracts, books, receipts, and different formats can quickly turn into a multi-step process.

Continuous Scan makes this much easier.

Instead of splitting your job into multiple files, you can scan pages through the document feeder and then add additional pages using the platen glass, all into a single file. There’s no need to manually merge documents later, which saves time and reduces frustration.

For offices handling a mix of document types, this is one of the simplest ways to streamline scanning.

Scan documents of different sizes and orientations

When you’re scanning packets that include different paper sizes, things can get messy fast. Manually adjusting settings or breaking jobs into separate scans slows everything down.

With Mixed Original Sizes, the e-STUDIO automatically detects each page’s size and orientation as it scans. That means everything is captured correctly in a single file, without extra steps or adjustments.

For teams working with varied document types, it’s an easy way to keep files accurate and consistent without adding time to the process.

Spend less time at the device

Standing at the MFP navigating menus just to access a USB drive is something most users deal with regularly.

The USB Auto Launcher removes that extra effort.

As soon as you plug in a USB device, the system automatically displays its contents. That means faster access to print files or save scans without tapping through multiple screens.

Note: This feature is available but may require installation by a service technician or Professional Services.

It’s a small change, but one that keeps work moving.

Turn your MFP into a communication tool

Your e-STUDIO device can do more than handle documents. It can also help keep your team informed.

With the Idle Screen feature, you can display messages directly on the home screen. This can be used for reminders, announcements, or simple updates that everyone in the office will see.

For teams, it’s an easy way to share information without relying on additional tools.

Stop losing time searching for files

One of the most common frustrations with scanning is finding files later, especially when they aren’t named clearly.

Searchable PDF solves that problem by making the text inside your documents searchable.

Save time and reduce frustration by allowing your system to scan directories and repositories for keywords within files, giving you faster, smarter file discovery.

Make everyday tasks one-touch simple

Repetitive tasks can slow down even the most efficient teams.

Programmable buttons 1 & 2 allow you to create shortcuts for frequently used workflows right on the device. With a single tap, users can access the functions they use most often.

Before using these buttons, an administrator will need to configure them in TopAccess.

This not only speeds things up, but also makes the device easier to use for everyone in the office, regardless of experience level.

Combine paper and digital files without extra tools

Working with both physical and digital documents is part of everyday business, but combining them can be a hassle.

With e-Filing, you can store, manage, and merge files directly on your e-STUDIO device.

That means you can scan a paper document, bring in an existing digital file, and combine them into one file without leaving the MFP. It’s a straightforward way to keep documents organized and accessible.

Small changes can make a big impact

The most valuable e-STUDIO features are often the ones that quietly improve how work gets done. They reduce extra steps, eliminate common frustrations, and help your team stay focused.

For offices, that can mean less time at the device, fewer workarounds, and faster access to the information that matters.

If you’re only using your e-STUDIO MFP for basic print and scan, now is the time to explore what else it can do.

Want help setting up these features on your e-STUDIO device? Contact your Toshiba representative to get started.

English (US)
English (US)