Join us at Elevate Live! in Las Vegas or online June 12-16.  Register Now

Leadership

A4 vs. A3 printers: Which is right for your office?

Robert Covington / September 14, 2026
Toshiba MFP in an office setting.

When choosing office printing equipment, businesses often have to decide between A4 and A3 devices. While both can support printing, copying and scanning, they serve different needs.

So, which is better: an A4 or A3 printer or multifunction printer (MFP)?

The answer depends on several factors, including print volume, available space, required features, cost per page, security and how employees work. For many organizations, the best approach is not choosing one format over the other. Instead, a combination of A4 and A3 devices can create a more efficient and cost-effective print environment.

What is the difference between A4 and A3 printers?

The primary difference between A4 and A3 devices is the size of paper they can handle.

A4 devices are designed primarily for standard office documents and smaller workgroups. They typically have a smaller footprint and lower acquisition cost, making them well suited for individual employees, small departments and remote workers.

A3 devices can handle larger media sizes in addition to standard A4 documents. They also tend to offer higher-duty cycles, more finishing options and advanced features. As a result, A3 MFPs are often a better fit for larger workgroups, higher-volume environments and organizations that need more advanced document workflows.

However, the difference is no longer simply about paper size. Modern A4 MFPs continue to add features and capabilities that once were primarily associated with larger A3 devices.

Why A4 devices have become more important

The way people work has changed significantly in recent years.

Hybrid and remote work have reduced the number of employees who regularly work from a traditional office. At the same time, organizations have continued to digitize documents and workflows.

That creates an interesting balance.

Employees may print less overall, but they still need access to basic printing, copying and scanning when a physical document is necessary. An A4 device can provide those capabilities without requiring the space or investment associated with a larger A3 MFP.

For a remote employee, for example, an A4 MFP can provide the core functions needed for occasional office tasks while keeping the device compact.

The same principle can apply inside the office. Smaller teams and reduced headcounts can make it unnecessary to place a large A3 device in every department.

Why A3 MFPs remain important

The shift toward A4 does not mean A3 devices have become obsolete.

A3 MFPs continue to provide important advantages for organizations with higher print volumes or more complex document requirements.

They can offer:

  • Higher-volume performance
  • Advanced finishing capabilities
  • Larger and more capable document feeders
  • Expanded workflow and scanning options
  • More robust user interfaces
  • Lower cost per page in the right environment
  • Greater opportunities for document workflow solutions

For organizations that regularly produce large volumes of documents, the higher acquisition cost of an A3 MFP can make sense when the device’s capabilities and cost per page justify the investment.

A3 devices can also serve as a digital onramp, connecting physical documents with digital workflows and business applications. That makes the device more than a printer. It becomes part of the organization’s overall document strategy.

Should an office use A4 and A3 devices together?

In many cases, yes.

A mix of A4 and A3 devices can help organizations right-size their print environment based on how different employees and departments actually work.

For example, a business might use an A3 MFP in a high-volume department that requires advanced finishing while providing A4 devices to smaller workgroups with lower print volumes.

This approach can help balance device capabilities with actual demand.

Managed Print Services can also help organizations determine where each device belongs. By analyzing print volume, usage patterns, features and cost per page, businesses can identify opportunities to place the right device in the right location.

The goal is not to have the most powerful device everywhere. The goal is to have the right device where it provides the most value.

Are A4 MFPs replacing A4 printers?

A4 MFPs are becoming an increasingly important option for modern offices because they combine multiple functions in a single device.

Instead of providing separate devices for printing, copying and scanning, an A4 MFP can bring those capabilities together.

That can also create opportunities for workflow automation.

For example, an employee might scan a document and send it directly to a cloud application, business system or designated workflow instead of manually scanning the document, emailing it to themselves and uploading it later.

As businesses look beyond basic printing, these types of solutions can make an A4 MFP more compelling than a standalone printer.

How important is color printing?

Color remains an important consideration, but organizations often want to control how and when employees use it.

Color printing can improve presentations, marketing materials and other business documents. However, unrestricted color printing can also increase printing costs.

That is why many organizations use print management features to monitor and control color usage.

For example, businesses may require users to enter a department code before printing in color. Administrators can also establish quotas or usage limits.

This allows organizations to maintain access to color when it provides business value while keeping unnecessary costs under control.

Why does the size of an A4 device matter?

The smaller footprint of an A4 device can be a major advantage in today’s office environment.

Office space is valuable, particularly as organizations rethink how much dedicated space employees and equipment need. A compact device can fit into locations where a larger MFP may not be practical.

However, footprint should not be the only consideration.

Businesses should also evaluate how often employees need finishing capabilities such as stapling, how much paper they print and whether the device needs to support advanced workflows.

In some environments, an A3 MFP with an integrated finishing option may make sense. In others, a compact A4 device may provide everything employees actually need.

What makes today’s A4 MFPs different?

Today’s A4 MFPs have continued to close the capability gap with larger devices.

Several improvements make modern A4 devices more useful for business environments, including:

  • Larger, more intuitive user interfaces
  • Improved document feeder capabilities
  • Better scanning performance
  • Stronger workflow integration
  • Support for business applications and cloud services
  • Improved security features
  • More advanced device management

These capabilities allow organizations to look at A4 devices as more than low-cost alternatives to A3 equipment.

The continuing development of A4 technology could make the distinction between the two formats increasingly about media size rather than overall functionality.

How does hybrid work affect A4 and A3 device selection?

Hybrid work has changed where and how employees use printing equipment.

Employees may work from home several days a week but still need printing and scanning capabilities when they are in the office. At the same time, organizations need to consider the security and management implications of employees purchasing inexpensive printers independently.

A professionally managed print environment can give organizations greater control over device security, support, supplies and total cost of ownership.

For some businesses, a combination of A3 devices in shared office spaces and A4 devices for smaller workgroups or home offices can provide a practical solution.

The key is to look at the entire environment rather than evaluating each device in isolation.

A4 vs. A3: Which should your business choose?

There is no universal answer to the A4 vs. A3 question.

An A4 device may be the better choice when an organization needs a compact solution for lower-volume printing, smaller workgroups or hybrid employees.

An A3 MFP may be the better choice when an organization requires higher print volumes, advanced finishing, more robust workflows or lower cost per page at higher usage levels.

For many businesses, the best solution is a combination of both.

The right strategy starts with understanding how employees actually print, scan and manage documents. From there, businesses can evaluate device capabilities, volume, cost per page, security, workflow requirements and available space.

Rather than asking whether A4 or A3 is better, the more useful question is:

Which device provides the right capabilities for each employee and workgroup?

That shift in perspective can help businesses build a more efficient, secure and cost-effective print environment.

Frequently asked questions about A4 and A3 printers

Is an A4 printer better than an A3 printer?

Neither format is universally better. A4 devices are generally suited to smaller workgroups, lower print volumes and space-conscious environments, while A3 devices can provide greater capacity, finishing options and advanced functionality for higher-volume environments.

What is the main advantage of an A4 MFP?

An A4 MFP combines printing, copying and scanning in a compact device. Modern A4 MFPs can also support document workflows, cloud applications and other business solutions.

Why do businesses still use A3 MFPs?

Businesses continue to use A3 MFPs because they can support higher print volumes and more advanced document workflows. They can also provide features such as finishing and robust document handling that may be important for larger workgroups.

Can a business use both A4 and A3 devices?

Yes. A combination of A4 and A3 devices can help businesses match equipment to the needs of different departments, workgroups and employees.

Does hybrid work increase the need for A4 devices?

Hybrid work can increase the need for smaller A4 devices because employees may need basic printing and scanning capabilities without requiring the capacity of a larger A3 MFP.

How should a business choose between A4 and A3?

Businesses should consider print volume, cost per page, device footprint, required features, finishing needs, security, workflow requirements and how employees work. An assessment of the entire print environment can help determine the right mix of devices.

English (US)
English (US)