Join us at Elevate Live! in Las Vegas or online June 12-16.  Register Now

Security

Is Your Print Server Quietly Becoming a Risk?

Gerry Gerhardt Headshot
Gerry Gerhardt / June 3, 2026
An IT professional working on a print server

For many IT organizations, the print server is one of the last remaining on‑premises systems quietly doing its job in the background. Users can print. Tickets are manageable. Nothing appears obviously broken. Because of that, printing infrastructure often receives far less attention than other core systems.

The challenge is that print environments rarely fail all at once. Instead, they tend to become fragile over time, especially as operating systems, security models, and device management practices evolve. What once felt stable can gradually turn into something unpredictable—breaking during routine changes like Windows updates, new PC rollouts, or printer replacements.

This article explains what makes a print server risky, why that risk is increasing, and what IT leaders should be thinking about before small issues turn into larger operational problems.

Why print servers are easy to ignore

Print servers occupy an unusual place in enterprise IT:

  • They are business‑critical
  • They are often old
  • They are rarely modernized unless something breaks

In many environments, the print server is:

  • One of the oldest Windows servers still in production
  • Maintained with legacy drivers or custom scripts
  • Dependent on configurations that few people want to touch

As long as nothing changes, this can feel acceptable. But modern IT environments change constantly—and printing is more sensitive to those changes than many teams realize.

What “risky” means in a print environment

A risky print server is not necessarily failing today.

In fact, many risky print servers:

  • Continue to print successfully
  • Accumulate technical debt quietly
  • Become increasingly sensitive to routine change

Risk typically shows up when something new happens:

  • A Windows update is applied
  • A new PC is issued
  • Security policies are tightened
  • A printer model is refreshed

When that happens, printing may still work—but features disappear, queues behave inconsistently, or users require manual fixes that didn’t used to be necessary.

The changing nature of windows printing

Over the last several years, Windows printing has undergone steady change as Microsoft works to improve security and reliability across the platform.

These changes include:

  • Reduced reliance on traditional third‑party print drivers
  • Increased emphasis on standards‑based printing
  • Tighter controls around driver installation and trust
  • New models designed to reduce attack surface

One example of this evolution is Windows Protected Print, which is part of Microsoft’s broader effort to modernize the Windows print stack. Windows Protected Print changes how drivers and printer features are handled and encourages more predictable, secure printing behavior.

These changes are generally positive. However, they also mean that older print server designs may not age well unless they are reviewed and aligned with where Windows printing is headed.

Where print server risk usually appears first

Print servers rarely fail during calm periods. Risk tends to surface during moments of change.

Common trigger points include:

New PC deployments
New Windows devices may behave differently than older machines, particularly in how printers and features are discovered or installed.

Printer replacements
Replacing hardware often exposes assumptions baked into scripts, queues, or driver packages that no longer apply.

OS updates and policy changes
Routine Windows updates or security policy adjustments can affect driver behavior and feature availability.

Security and compliance reviews
Print servers frequently raise flags during audits due to outdated configurations or inconsistent patching.

None of these scenarios are unusual. The issue is whether the print environment is resilient enough to handle them without disruption.

Why the warning signs are easy to miss

Printing problems rarely announce themselves clearly.

Instead, the warning signs are subtle:

  • A gradual increase in help desk tickets
  • More manual intervention after routine changes
  • Inconsistent behavior across similar devices
  • A growing list of “known quirks” no one wants to revisit

Because printing still works most of the time, these signals are often deprioritized. Over time, however, they add up and consume more operational effort than expected.

“Working today” is not the same as “ready for tomorrow”

One of the most common assumptions about print servers is that if they work today, they will continue to work tomorrow.

In reality:

  • Printing is tightly coupled to the operating system
  • Operating systems evolve continuously
  • Security expectations continue to rise

A print server that hasn’t been reviewed recently may not be broken—but it may be misaligned with the direction Windows printing is taking. That misalignment is where risk accumulates.

Questions IT leaders should be asking

You don’t need a full technical audit to begin understanding print server risk. It’s often enough to step back and ask:

  • How predictable is printing when devices or users change?
  • How dependent is our environment on legacy components?
  • How confident are we that printing will behave the same after future Windows updates?
  • How much time does the team spend maintaining printing relative to its business value?

If these questions are difficult to answer, that’s usually a sign the environment deserves closer attention.

A Better way to think about print server risk

Rather than asking:

“Is our print server broken?”

A more useful question is:

“How resilient is our print server to change?”

Resilient print environments:

  • Handle updates gracefully
  • Require minimal manual intervention
  • Behave consistently across devices
  • Fade into the background where they belong

Fragile environments:

  • Break during routine changes
  • Depend on outdated assumptions
  • Consume more time and attention over time

Understanding where your environment falls on that spectrum is the first step toward reducing risk.

Final thought

Print servers rarely get attention until something goes wrong. By then, the cost is already being paid in lost time, frustrated users, and reactive work.

Taking a moment to understand whether your print server is quietly becoming a risk can help prevent those issues before they surface. The goal isn’t to overhaul everything overnight—it’s to make sure printing remains secure, predictable, and boring.

In IT, boring is usually a sign things are working the way they should.

English (US)
English (US)