Toshiba e-STUDIO Series

	Copyright(c) 2004-2022 Toshiba Tec Corporation, All Rights Reserved.
			May 20, 2022

This product has the following restrictions and issues.  Please be sure to read this before using.

--------------------------------------------------------------------------------
Installation
--------------------------------------------------------------------------------

The Toshiba e-STUDIO series products are as follows:
e-STUDIO6550C Series
e-STUDIO4540C Series
e-STUDIO6530C Series
e-STUDIO4520C Series
e-STUDIO850/853 Series
e-STUDIO451c/453c Series
e-STUDIO452/453 Series
e-STUDIO282/283 Series
e-STUDIO3510c Series
e-STUDIO455 Series
e-STUDIO855 Series
e-STUDIO456 Series
e-STUDIO856 Series
e-STUDIO2550C Series
e-STUDIO407CS Series
e-STUDIO527S Series
e-STUDIO507 Series
e-STUDIO857 Series
e-STUDIO6570C Series
e-STUDIO5005AC Series
e-STUDIO5008A Series
e-STUDIO7506AC Series
e-STUDIO8508A Series
Loops-LP30_e-STUDIO306LP
e-STUDIO307LP_Loops-LP301
e-STUDIO5008LP_Loops-LP50 Series
e-STUDIO5015AC Series
e-STUDIO5018A Series
e-STUDIO7516AC Series
e-STUDIO8518A Series
e-STUDIO400AC Series
e-STUDIO6525AC Series
e-STUDIO6528A Series
e-STUDIO7527AC Series
e-STUDIO9029A Series

--------------------------------------------------------------------------------
e-STUDIO e-Filing Backup/Restore Utility	Version 4.1.21.0
--------------------------------------------------------------------------------

Issues
======

1. Accessing performance may decline when the e-Filing Box contains many documents. 

2. On Windows Vista, please do not select "Desktop" at the top in the dialog box while saving a backup file on the desktop in a user's computer.
   You can save the backup file on the desktop in a user's computer if the following path is selected "Desktop"->"User's computer name"->"Desktop."

3. The length of the specified absolute path to "Target file" should not exceed 250 bytes.

4. When us use SNMP V3, be sure to start Local Discovery and configure SNMP V3 settings after updating software via CD V3.1.42.0/V3.1.42.1/V3.1.42.3 for the e-STUDIO6530C/e-STUDIO4520C series.

5. Transition into the energy saving mode is not performed during backup/restoring.

Troubleshooting
===============

1. Cannot find the MFP.
[Problem Description]
Cannot find the MFP even when the Local Discovery or Network Discovery feature is used.

[Corrective Action] 
Please check the following: 
- The MFP and your PC are correctly connected to the TCP/IP network.
- The MFP is connected to a different subnet and the default gateway setting is correct.

[NOTE]
- e-Filing Backup/Restore Utility does not support the GL-1010 or GL-1020 controller.  These controllers cannot be found by Local Discovery. 

2. Cannot connect to the MFP found by the Local Discovery
[Problem Description]
The Local Discovery finds the MFP, but you cannot connect to it.

[Corrective Action]
1. Make sure Microsoft Internet Explorer 5.5 or later is installed.
2. Make sure the Proxy settings on the Microsoft Internet Explorer have been made correctly so that your PC can connect to the MFP.
3. Make sure Microsoft Internet Explorer is not in the off-line mode. If it is in off-line mode, change it to the on-line mode.

[NOTE]
- Connection to the MFP may fail when too many PCs are connected to the MFP at the same time.  Please try to connect to the MFP again later.

3. Error Message 
When an error message appears, solve a problem with reference to the following descriptions. 

[Error Message]
"Invalid Administrator Password.
 Please enter correct Administrator Password."

[Corrective Action]
The administrator password entered is incorrect.  Please enter the correct administrator password.

[Error Message]
"Another user is using the MFP.
 Please retry later."

[Corrective Action]
Another user is using the MFP.  Please retry later after a while.

[Error Message]
"Failed to establish connection with Box.
 Please retry later."

[Corrective Action]
Initialization of e-Filing Box has not been completed.  Please retry later after a while.

[Error Message]
"Connection to MFP has aborted.
 Device is not found."

[Corrective Action]
Either the MFP power is turned off or the network is initializing.  Please turn off the MFP power and turn it on again, then retry later after a while. 

[Error Message]
"Internal Error Occurred."

[Corrective Action]
An internal error has occurred.  Please turn off the MFP power and turn it on again, then restart the application and retry.

[Error Message]
"Time Out Occurred.
 Please Refresh."

[Corrective Action]
A session timeout has occurred.  Select "View"=>"Refresh" from the menu. 

[Error Message]
"Maximum Document Limit reached under xxxx
 Please Delete or Move some of the documents before restoring"

[Corrective Action]
The number of documents has reached the maximum limit during Restore.  Please delete unnecessary documents and retry. You can create up to 400 documents in each box and folder.

[Error Message]
"Maximum Folder Limit reached under xxxx
 Please Delete or Move some of the Folders before restoring."

[Corrective Action]
The number of folders has reached the maximum limit during Restore.  Please delete unnecessary folders and retry.  You can create up to 100 folders in each box.

[Error Message]
"Selected Boxes to be Backed-up have been deleted,
 Please reselect Boxes"

[Corrective Action]
The selected boxes were deleted while waiting Automatic Backup.
Please select the boxes again and retry.

[Error Message]
"Disk is Full."

[Corrective Action]
The backup server or the PC's hard disk is full.  Please delete the unnecessary data using a delete function.  Retry after making sure that memory space is sufficient. 

[Error Message]
"Insufficient Memory."
"Disk in MFP is full. 
 Please select less number of Boxes."

[Corrective Action]
The MFP's hard disk is full.  Please delete the unnecessary data using a delete function and retry.  To execute Restore, decrease the number of boxes to be selected and retry.

[Error Message]
"Version is unsupported."

[Corrective Action]
The backup file of the old version is found.
Please contact your dealer for support to update the MFP's ROM version.  

[Error Message]
"Higher version is detected.
 Please upgrade the application."

[Corrective Action]
 The backup file of the latest version is found.
 Please update the application.

[Error Message]
"Cannot Connect to Box in offline mode. 
Please change mode to online from Internet Explorer."

[Corrective Action]
Internet Explorer is in offline mode.
Deactivate the offline mode in Internet Explorer.

[Error Message]
"Network Paths are not supported.
Please map the Network Folder with Local Drive and provide the local drive path."

[Corrective Action]
Designate a folder in the active computer to store the backup files.

[Error Message]
"Invalid Path Information.
Please provide a valid path."

[Corrective Action]
Invalid file name or folder name is entered. 
Enter a valid path. 

[Error Message]
"The Backup files could not be restored.
Disk in MFP is full.
Please increase the e-Filing space available."

[Corrective Action]
The MFP hard disk is insufficient to restore the backup files.  Delete unnecessary data using the delete function, and retry again.

[Error Message]
"The Backup files could not be restored.
Operation Timeout Occurred.
Please retry later."

[Corrective Action]
A session timeout has occurred.  
Retry this operation later.

--------------------------------------------------------------------------------
Trademarks
--------------------------------------------------------------------------------

- The official name of Windows Vista is Microsoft Windows Vista Operating System.
- Microsoft, Windows, and the brand names and product names of other Microsoft products are trademarks of Microsoft Corporation in the US and other countries.
- Other company names and product names in this manual are the trademarks of their respective companies.